Technical FAQs

Ask a Question

How to Add, Modify, or Remove a Logical device for an ECI850 in CET850

How to Add a logical device:
1. In the tree view, select an IED element whose type is ECI850 Sepam Server.
2. In the menu bar or in the contextual menu, click Add > Logical Device.
3. Set the fields of the Add Logical Device window according to the rules described in the Logical Device identification section.
4. Click OK to validate the operation
a. A New Logical Device element is added in the tree view inside the ECI850 Sepam server.

How to Modify a logical device:
1. Select in the tree view the Logical Device to be modified.
2. In the property view, select an attribute and click Modify in the contextual menu. A dialog box opens, displaying a table with the attributes and their values.
3. Click the Attribute Value column fields to modify them.
4. Click OK to validate the modification.
a. The logical device parameters are updated

How to Delete a logical device:
1. Select in the tree view the Logical Device you want to remove.
2. In the menu bar or in the contextual menu, click Edit > Delete or press the DEL key.
a. The logical device is removed from its ECI850 Sepam Server.

AEDL3

 
Legacy KB System (APS) Data: RESL204863 V1.0, Originally authored by MiZe on 03/19/2011, Last Edited by MiZe on 03/19/2011
Related ranges: Sepam accessories
Was this helpful?
What can we do to improve the information ?