Technical FAQs

Ask a Question

What programs are used to configure an IEC61850 for SEPAMs?

Product Line   
SEPAM 80
SEPAM 40

Environment    
Communication setup  

Resolution   
There are two different programs that can be used to program the IEC61850 configuration file for the SEPAM's
1. To build a simple configuration file use SFT2841.  To get SFT2841 download file just clear here.
2. To build a highly customized configuration file use CET850.  To get CET850 download file just clear here.

Was this helpful?
What can we do to improve the information ?