Technical FAQs

Ask a Question

What sections of the IEC61850 are the ECI850 and ACE850 modules compliant with?

The ECI850 and the ACE850 modules are compliant with the following sections:
1. IEC61850-6
2. IEC61850-7-1
3. IEC61850-7-2
4. IEC61850-7-3
5. IEC61850-7-4
6. IEC61850-8-1

AEDL3


Legacy KB System (APS) Data: RESL204835 V1.0, Originally authored by MiZe on 03/17/2011, Last Edited by MiZe on 03/17/2011
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software)
Was this helpful?
What can we do to improve the information ?