Technical FAQs

Ask a Question

What does Neg stand for under logic inputs in SFT2841?

Product Line  
SEPAM 20
SEPAM 40
SEPAM 50
SEPAM 80

Resolution   
There is a Neg box for the logic inputs in SFT2841. This option, if checked, allows one to wire the input as a negative input. For instance, 1 is normally considered to be high, if you checked Neg, you would effectively be telling the relay that 0 is high.

 

Was this helpful?
What can we do to improve the information ?