Technical FAQs

Ask a Question

Typical 3-line drawings for Sepam Series 20, 40 and 80 current and voltage input connections

Goals and Symptoms

Typical 3-line drawings of Sepam 20/40 Feeder, Sepam 20/40 Main and Sepam 80 Main/Feeder.

Causes and Fixes

See attachment

Legacy KB System (APS) Data: RESL203669 V1.0, Originally authored by MiZe on 10/09/2010, Last Edited by MiZe on 10/09/2010
Related ranges: Sepam series 80, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?