Technical FAQs

Ask a Question

What types of terminal blocks are available for the Sepam Relay?

The Sepam Series 20, 40 & 80 base units are available with 2 different types of terminal blocks: Screw Type (CCA620) & Ring Lugs (CCA622).
By default, relays sold in North America are shipped with ring lug connectors as the standard terminal block, unless the screw type connectors (optional) are specified. The MES114 & MES120 I/O modules are all sold with screw type terminal blocks (ring lugs aren't available).


Screw Type


Ring Lugs

Was this helpful?
What can we do to improve the information ?