Technical FAQs

Ask a Question

VIGI PA: can we use the MITOP Output of the EPAMI MI 321 for the self-tripping of the MC SET circuit breaker?

Goals and Symptoms

VIGI PA: can we use the MITOP Output of the EPAMI MI 321 for the self-tripping of the MC SET circuit breaker?

Causes and Fixes

Yes we can with the old generation of MC SET 4 (with GMH order like the 24 KV) because the MITOP is more sensitive than the new MITOP of MC 500 (not yet approved by EDF).

AEDL3


Legacy KB System (APS) Data: RESL201037 V1.0, Originally authored by DaMi on 01/22/2010, Last Edited by DaMi on 01/22/2010
Related ranges: VigiPA PA
Was this helpful?
What can we do to improve the information ?