Technical FAQs

Ask a Question

SFT2841 displays the message "A more recent version of the Logipam software is available" in the Logipam settings page. What does this mean?

The message "A more recent version of the Logipam software is available" in the Logipam settings page of SFT2841 means that the .bft configuration file that was created in SFT2885 has been updated since the last upload. SFT2841 cannot upload the file into the relay every time changes are made to it in SFT2885, but it will notify the user that a more recent copy is available by displaying this message on the bottom of the Logipam settings page:


In order to upload the more recent copy into the relay, the user must click "Update". This will automatically synchronize the SEPAM relay with the latest configuration file that had been created using SFT2885 Logipam software.

AEDL3


Legacy KB System (APS) Data: RESL200918 V1.0, Originally authored by MiZe on 01/06/2010, Last Edited by MiZe on 01/06/2010
Related ranges: SFT 2885 (Sepam series 80 Logipam)
Was this helpful?
What can we do to improve the information ?