Technical FAQs

Ask a Question

Can Remote Control be enabled from the advanced UMI of the Sepam Series 20, 40, 60 and 80 Relay?

For the Sepam Series 20 and 40 relay, "remote control" can be activated by navigating through the front face of the Sepam relay.
Go to general settings -> Modules -> Modbus. Scroll down until the remote control screen appears.

Note: "SBO" means Select Before Operate

For the Sepam Series 60 and 80 relay, "remote control" cannot be activated by navigating through the front face.
In order to activate this setting, connect to the relay using the SFT2841 Software kit with the CCA783 cord.
"Remote Settings" is located under the "General Characteristics" tab of SFT2841.


Date Created: March 13, 2008
Last Revised: October 21, 2008
Original Author: JJ
All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL193010 V1.0, Originally authored by PhHa on 10/26/2008, Last Edited by PhHa on 10/26/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software), Sepam series 80, Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?