Technical FAQs

Ask a Question

Are logical equations lost in the Sepam Series 40 , 60 or 80 relay after reloading factory settings using SFT2841?

When reloading factory settings using SFT2841, all parameter settings will be erased except for logical equations.

If removing these equations is necessary, they must be removed manually using the SFT2841 commissioning software.



If, for example, a new configuration file (without logic equations) is loaded to a Sepam device (w/ logic equations), the logic equations in the Sepam device are erased and the Logic Equation screen becomes blank.



AEDL3


Date Created: February 25, 2008
Last Revised: September 5, 2008
Public
Original Author: JJ
All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL192716 V1.0, Originally authored by PhHa on 09/06/2008, Last Edited by PhHa on 09/06/2008
Related ranges: SFT 2841 - SFT2848 (Sepam series 20, 40, 80 software), Sepam series 80, Sepam series 40
Was this helpful?
What can we do to improve the information ?