Technical FAQs

Ask a Question

Memory Cartridge Install Sheet, Instruction Bulletin (ANSI), 63230-216-247A1

The MMS020 memory cartridge provides the application-specific factory settings and overall processing power for Sepam Series 80 relays. By encapsulating the relay settings, a Sepam Series 80 relay can be retrofitted for alternate applications.
Plug-and-play installation and two attachment screws make the memory cartridge easily accessible and removable from the front of the Sepam Series 80 relay.


see attachment:

63230-216-247_MMS020_InstallSheet.pdf



Keywords:
63230216247

 AEDL3


  • Date Created: February 26, 2008
    Last Revised: February 26, 2008
    Public
    Original Author: JJ
    All content © 1992-2008 Schneider Electric

Legacy KB System (APS) Data: RESL191287 V1.0, Originally authored by PhHa on 02/27/2008, Last Edited by PhHa on 02/27/2008
Related ranges: Sepam series 80, Sepam accessories




 
Was this helpful?
What can we do to improve the information ?