Technical FAQs

Ask a Question

Where is the GSD file located for a Profibus 7300?

The GSD (Generic Station Description) file is used only for the ION 7300 meter with Profibus communication option.This file is required for the initial setup of the meter.
7300 Profibus - Installation Package.zip


Document Change History

Date and Initials Comments
2012-02-01 DRM * Reference to a now defunct FTP site and added the relevant document as an attachment instead.
2010-11-04 DRM * Changed range association away from "Communication application \ Profibus" in preparation for the removal of this range and the product family under which it is classified.




Applies To: ION 7300, Profibus protocol ("Other protocols" category)
Public
All content © 1992-2010 Schneider Electric


Legacy KB System (APS) Data: RESL190288 V3.0, Originally authored by KBAdPM on 12/08/2007, Last Edited by DaMi on 02/02/2012
Related ranges: Other protocols, ION7300
Was this helpful?
What can we do to improve the information ?