Technical FAQs

Ask a Question

What are the differences of SFT2826 software used with Sepam 1000+ range?

SFT2826 is an unique software for data files restitution uploaded from Sepam 2000 and Sepam 1000+ ranges: There is so no basic difference (unique software).
The only difference for using this software comes from the number and nature of data saved in COMTRADE files, these files being adapted to each range : Sepam 2000, Sepam 1000+ series 20, Sepam 1000+ series 40.

Details of the versions :
..V9826 : original version
..V9952 : suppression of the installation locking (n° of licence), suppression of the 16 bits version
..V0007 : addition of a missing .dll file.
..V0051 : modification of the start up of the software in window mode instead of full screen
..V0118 : addition of the Sepam series 40 screens


Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Original Author: FK

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166711 V2.0, Originally authored by FrKr on 06/18/2008, Last Edited by DaMi on 06/18/2008
Related ranges: Sepam 2000, SFT 2826 (OPG display), Sepam series 40, Sepam series 20
Was this helpful?
What can we do to improve the information ?