Technical FAQs

Ask a Question

Delete: What are the advantages of the new MET148-2 temperature module?


The new MET148-2 module which replaces the old MET148 may be used to connect 8 temperature APS_SENSORS for the measurement and protection of temperatures.

It has been available since May 2002 and provides the following:

- replacement of the MET148 already available for Sepam series 20 and series 40

- improvement of temperature measurement operating dependability and reliability

- use of 2 modules with Sepam series 40 (reminder: only 1 module with Sepam series 20): with 2 modules, set up the address of each module, with the power off.

The old module used alone is still compatible with the 2 Sepam series 20 and series 40 devices.
 

Last Revised: 30 June 2008 by DRM

Applies To: Sepam 1000+ (Series 20 and Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166641 V3.0, Originally authored by LaVI on 06/18/2008, Last Edited by DaMi on 07/01/2008
Related ranges: Sepam series 20, Sepam series 40
Was this helpful?
What can we do to improve the information ?