Technical FAQs

Ask a Question

What are the advantages of the new MET148-2 temperature module?

The new MET148-2 module which replaces the old MET148 may be used to connect 8 temperature APS_SENSORS for the measurement and protection of temperatures.
It has been available since May 2002 and provides the following:

- replacement of the MET148 already available for Sepam series 20 and series 40

- improvement of temperature measurement operating dependability and reliability

- use of 2 modules with Sepam series 40 (reminder: only 1 module with Sepam series 20): with 2 modules, set up the address of each module, with the power off.

The old module used alone is still compatible with the 2 Sepam series 20 and series 40 devices.

Re-published to revised security level: 17 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)


All content © 1992-2008 Schneider Electric

Was this helpful?
What can we do to improve the information ?