Technical FAQs

Ask a Question

How to save of alarm message histories?


The saving of alarm message histories can only be done by a remote monitoring and control system since this is the only effective means of saving in a substation that includes several Sepam devices. The devices are connected in a Modbus network to the remote monitoring and control system.

However, there is a simple but effective way to save individual Sepam histories, if the customer accepts to connect locally to the Sepam with a PC.

The procedure is described below:

 

Sepam series 20


The only possibility consists of saving a screen copy as follows:

- SFT2841 is connected to the Sepam

- select the diagnosis icon, history tab

- save the screen by pressing ALT + Print Screen

- paste in a Word filing by pressing CTRL+V

- name and save the file

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166603 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 20, Sepam series 40
Was this helpful?
What can we do to improve the information ?