Technical FAQs

Ask a Question

Is Sepam series 80 remote setting protected by a password?

 

  • Yes, Sepam series 80 remote control and remote setting can be protected by passwords.
  • A first password may be used to protect remote control and a second one to protect remote setting.
  • Different passwords can be used for each communication port.
  • The passwords are set up via the SFT2841 using the "Sepam unit" icon.

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam Series 80

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166602 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 80
Was this helpful?
What can we do to improve the information ?