Technical FAQs

Ask a Question

What is the sampling frequency of Sepam series 80?


The sampling frequency is controlled by the network frequency, between 25Hz and 65Hz.

For measurements (except for RMS and THD) and protection functions, the sampling frequency is 12 times the electrical network frequency, i.e. 600 Hz for 50 Hz networks, 606 Hz for 50.5 Hz networks and 720 Hz for 60 Hz networks.

For RMS and THD measurements, the sampling frequency is 36 times the electrical network frequency

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam Series 80

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166600 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 80
Was this helpful?
What can we do to improve the information ?