Technical FAQs

Ask a Question

What information is saved in the event of a Sepam series 80 power failure?


The saving of information depends on whether or not the battery is present. In the event of a Sepam series 80 power failure, certain data will only be saved if the battery is present.

The data listed below are only saved if the battery is present:

  • Peak demand current
  • Peak demand active power
  • Peak demand reactive power
  • Tripping context
  • Tripping current
  • Disturbance recordings
  • Starting current
  • Starting time
  • Alarm message history
  • Date and time


The data listed below are saved with or without a battery present:
  • Calculated active energy
  • Calculated reactive energy
  • Number of trips (phase overcurrent and earth fault)
  • Machine heat rise
  • Running hours counter and operating time
  • Cumulative breaking current
  • Number of operations
  • Operating time
  • Charging time
  • Number of rackouts

Important: All the data contained in the cartridge are saved.

Re-published to revised security level: 18 June 2008 by DRM

Applies To: Sepam Series 80

Public

All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL166578 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 80
Was this helpful?
What can we do to improve the information ?