Page not found...

Increase your level of satisfaction


Gaining time in all of a project’s development and installation phases is vital if installation commissioning dates are to be met.


Go for simplicity


  • Measure, manage, analyse and diagnose all the applications in an installation.
  • A comprehensive range with a relay that corresponds exactly to your requirements.
  • Designed for the following applications:
    - substation,
    - transformer,
    - generator,
    - capacitor bank,
    - busbar,
    - motor.
  • Management of the functions needed for each application (protection, measurement, control, temperature, etc.)
     
 
A range of solutions for all applications
 
For simple application
 
     
Modular construction
Configure it with
peace of mind
Communicate:
be open
 
Sepam’s modular architecture means it can be easily adapted to your requirements
> find out more
 
 
 
A single, user friendly and comprehensive PC configuration software.
> find out more
 
 
 
Sepam uses the market’s standard communication protocol.

> find out more
 

   
 

190

Schneider Electric has a presence in 190 countries


48 h

Sepam availability throughout the world


A requirement for quality
    • Design based on operating dependability studies.
    • Design meets IEC 61508 functional safety requirements.
    • ISO9001 certified development and production.
  • Manufacturing methods that respect the environment (ISO14001).