Automation and Control
News: Automation and ControlSave up to 26% versus traditional I/O with the Advantys ETB family of IP67 I/O modules.
Advantys ETB: new IP67-rated I/O modules for harsh environments
The Advantys range of distributed I/O has recently been expanded to include 2 new IP67-rated Ethernet I/O modules for use with Modbus TCP/IP or EtherNet/IP. The new modules are called Advantys ETB, for Ethernet Terminal Block. These new modules combine the functionality of block I/O with an embedded 2-port Ethernet switch and are used in applications where I/O is mounted directly on equipment, without requiring an enclosure. Applications
Industries
PLC compatability
Useful links
|