Automation and Control

News: Automation and Control

RFID innovations in conveying sectors

 

The new patented RFID systems provide high performance and innovative automatic identification solutions for the conveying and handling sector

The new RFID field expanders XGFE, used in conjunction with OsiSense XG stations, offer high performance solutions that enable : 

  • Dialogue with RFID tags across the entire width of the conveyor
  • Increasing the dialogue distance between the station and the tag
  • Higher passing speeds of the tags

Connection boxes XGSZ33 mount directly on the machine and easily enable the interfacing of OsiSense XG stations to Modbus, Ethernet TCP/IP and PROFIBUS-DP networks