• Default Alternative Text

    Why a Smart City?

Default Alternative Text

Efficient City Challenges

From rapid population growth to expanding emergency response systems to aging infrastructures, efficient cities will need to find innovative solutions to these complex problems, despite limited budgets.
  • Solutions

    A truly efficient city requires performance optimization, integration, and investment prioritization to maximize value. This enables a sustainable community with reduced environmental consequences to improve quality of life.

  • Value Proposition

    In less than 40 years, 70% of the world’s population will reside in cities. Urban centers need to become efficient, livable, and sustainable, in both the short and long term, by involving city, citizens and businesses.

  • Differentiation

    Our 5-step approach:

    1. Vision: setting the goal and roadmap

    2. Solutions: technology to improve efficiency

    3. Integration: combining IT and OT systems

    4. Innovation: building the business model

    5. Collaboration: with global and local stakeholders

Looking up at skyscrapers under construction

The Smart City Cornerstone: Urban Efficiency

Benefits

  • Forest/Wood view, sustainability reporting, environment
    • Up to 30% energy savings.
  • Default Alternative Text
    • Up to 20% reduction in water losses.
  • Default Alternative Text
    • Up to 30% reduction in street crime from CCTV security cameras.
  • Default Alternative Text
    • Up to 20% reduction in travel time and traffic delays.
  • Default Alternative Text
    • Plus, improved safety and higher quality of life.