• Default Alternative Text

    Learn more about EcoStruxure™ Facility Advisor

  • Resources

    • Sustainability consulting between two factory workers in bottling plant, food and beverage.

      Brochure
      Discover EcoStruxure™ Facility Advisor services

      Today facility management is about more than just ensuring the safety and functionality of a building’s physical structure. It’s also about cutting costs, saving time, ensuring comfort, and complying with regulations. Plus, budget cuts and increased pressure to achieve more with less has reduced the room for error – making modern facility management even more challenging.

      EcoStruxure™ Facility Advisor (formerly known as Facility Insights) services is a suite of managed services, outsourced to certified EcoXpert services partners.

      Read the brochure
    • Default Alternative Text

      PDF Presentation
      Introduction to EcoStruxure Facility Advisor services

      Services to improve facility performance and operations:

      - Expert services to analyze data
      - Recurrent reports to understand data
      - Expert support to optimize the facility
      - Multi-site comparison to focus on poorly performing sites
      - Recommendations to implement fast actions
      - Detection of abnormal consumption and parameters
      - Optimized data acquisition installed by our local partners
      Download the presentation
    • Default Alternative Text

      White paper
      How to design an efficient metering system

      Energy efficiency systems can increase property values, facilitate resale, and boost rental occupancy rates and yields. Many such systems are also cost effective to set up and guarantee rapid return on investment. One thing that all energy-efficiency measurements have in common is the need for reliable, accurate metering and monitoring of energy consumption. When it comes to commercial buildings, installing an effective WAGES (water, air, gas, electricity, steam) metering system can be a source of substantial energy and cost savings. Read the white paper
    • Dripping faucet with water drop

      Interactive PDF
      European Union Energy Efficiency Directive : standards and regulations in Europe.

      This document presents the different standards and regulations in Europe on Energy Efficiency in buildings.

      The European Union Energy Efficiency Directive includes the following :

      - Energy Audits standard (EN 16247)
      - Energy Management methodology (ISO 50001)
      - Energy Efficiency Services Process (EN 15900)
      - Impact of Building Automation, Controls and Building Management (EN 15232)
      Download PDF
    • Technician sitting in office running diagnostics in large data center

      e-Catalogue
      Access EcoStruxure™ Facility Advisor detailed datasheets

      Discover a full list of EcoStruxure Facility Advisor services, including: audits, connected services, managed services, service options, and on-demand services. Access catalog