Welcome to the Schneider Electric corporate Website

ENGLISH | FRENCH

Please choose your country or region to view available products.

Choose your country

      • PLANETIC (2013 – 2015)

        Establishing a technological platform for the information and communication technology (ICT) sector

      • Default Alternative Text

    Schneider Electric as a partner in an R&D collaborative project

    PLANETIC (2013 − 2015)

    The 3-year PLANETIC project aimed to provide a unified vision of the Spanish information and communication technology (ICT). The technological platform that answered the economic needs of the Spanish ICT sector was used to improve the sector's international positioning and serve as a common workplace for businesses and R&D centers.

    Co-founded by the Ministry of Economy and Competitiveness (Ministerio de Economía y Competitividad) under the 2008 – 2011 framework of the National Plan for Scientific Research, Development, and Technological Innovation (Pln Nacional de Investigación Científica, Desarrollo e Innovación Tecnológica) and the Influence subprogram (INF-2013-0254-430000 and PTR-2014-0367), the project had a €131K + €191K budget.

    Partners: ATOS, Telvent Energía, Tecnalia, CNM, and IK4

    For more information, visit http://www.planetic.es
    Nos conseillers sont disponibles pour répondre à vos questions de 8h00 à 18h00 du lundi au vendredi toute l'année.