Welcome to the Schneider Electric corporate Website

ENGLISH | FRENCH

Please choose your country or region to view available products.

Choose your country

      • certMILS (2017 - 2020)

        Compositional security certification for medium- to high-assurance COTS-based systems in environments with emerging threats

      • Default Alternative Text

    Schneider Electric as a partner in an R&D collaborative project

    certMILS (2017 - 2020)

    The 4-year certMILS (Compositional security certification for medium- to high-assurance COTS-based systems in environments with emerging threats) project aims to develop a security certification methodology for Cyber-physical systems (CPS). The project will employ a security-by-design concept originating from the avionics industry: Multiple Independent Levels of Security (MILS), which targets controlled information flow and resource usage amongst software applications. 


    The project includes an smart grid use case based on Schneider Electric Saitel RTU platform.

    Funded by  H2020 program of the European Commission (Grant agreement no: 731456), this project has an €5,6M budget and lasts from January 2017 to December 2020. 


    Partners: SYSGO, Schneider Electric, Technikon, Epoche & Espri, Thales, Atsec information security, Unicontrols, Universitaet Rostock, Elektrotechnicky Zkusebni Ustav, NXP. 


    For more information, visit http://www.certmils.eu

    "This project has received funding from the European Union’s Horizon 2020 research and innovation programme under grant agreement No 731456.”
    Nos conseillers sont disponibles pour répondre à vos questions de 8h00 à 18h00 du lundi au vendredi toute l'année.