• Default Alternative Text

    Building Automation & Control

    Our innovative Building Management, Power Management Systems and Small Building Control products provide a strong foundation for intelligent buildings that inspire occupant productivity and deliver optimal energy and operational efficiency.

  • Recognition Building energy management with innovation at every level

    Schneider Electric is proud to be again ranked number 1 in the Navigant Research Leaderboard Report: Building Energy Management Systems.

    Read more
    Default Alternative Text

    Building Facts

    • Blue smart city icon 42% of the world's energy is used in buildings.
    • Default Alternative Text 50% of energy used in buildings is wasted because of inefficient building management systems.
    • Blue tools icon In developed economies, at least half of the buildings expected to be in use in 2050 have already been built.
    • Default Alternative Text Only 25% of building costs are associated with capital expenses, while 75% of costs are used to operate a building over its life cycle.
    • Blue EcoXpert icon Only 20% of facility managers use 80% of the available capabilities in their building management systems.
    • Default Alternative Text 30% of energy used in buildings is waste.
    • Case Studies The Edge

      Schneider Electric helps make The Edge the world’s most sustainable office building.

      • SmartStruxure Solution Smart energy management for any size building
      • Critical power needs? Maximize and optimize your critical power needs.