• Default Alternative Text

    Insights on the connected enterprise

    Seeing the connections

    514410109-410x230

    New generation of IIoT-ready controllers reveals value hidden in process data

    Small problems that aren’t detected can add up to large profit shortfalls. More connected devices means more chances for problems to sneak through. For example, in a typical discrete/hybrid manufacturing plant, information on the performance of an asset such as a pump or motor is confined to the control level. Granular results are not available on all levels of the plant. So engineers and managers alike frequently lack the insight into operational performance they need to make faster, better decisions.

    Estimates say that lacking precise data on asset location, process status, and so on can cost up to three percent of yearly revenues. That can create a significant margin shortfall for the typical plant. The impact on the bottom line can be substantial.

    Fortunately, advanced Process Automation Controller [PAC] technology can help make granular production details available to interested users. The resulting operational visibility aids in stopping losses and delivering increased profitability.

    …lacking precise data on asset location, process status,
    and so on can cost up to three percent of yearly revenues..

    IIoT-ready PACs with built-in Ethernet allow seamless access to advanced collaborative and integrated automation architectures, and to object-oriented integration environments. It’s easy to link up controllers with other networks, and make any needed information visible throughout smart connected manufacturing enterprises.

    M580_IMG045-392x351

    The Modicon M580 Ethernet-enabled
    programmable automation controller (ePAC)
    platform from Schneider Electric possesses
    industry-leading processing and memory,
    as well as stronger embedded cybersecurity. 

    Example: if a controller reading exceeds preset parameters, the engineer or operator receives a text-message alert on their smartphone or tablet. They can then click through to the affected pump, motor, etc. Its location, coding, and full documentation are instantly available — without time-consuming trips to the control room or plant-floor PLC/PAC — for fast, efficient problem identification, investigation, and resolution. And fewer trips to the plant floor decrease the likelihood of adverse incidents and bring greater control of safety variables.

    So a quite-technical feature — transparent, open native networks embedded in an IIoT-ready PAC — can translate directly into real-world business improvements.


    For related information, click on any of the links below:

    [White paper series] Preparing for the IIoT,  exploring the impact
    Improving productivity in the connected enterprise - How the new generation of IIoT-ready controllers connects you to new levels of operational efficiency
    Facilitating project execution in the connected enterprise How the new generation of IIoT-ready controllers shorten time-to-value
    Seeing the Connections - How the new generation of IIoT-ready controllers reveals value idden in process data

    New value finder tool helps you discover $$ value hidden in plant assets
    Try it now